RS08 Assembler > Code Generation

Use this panel to specify the code generation options of the RS08 assembler.

The following image shows the Code Generation panel.

Figure 1. Tool Settings - RS08 Assembler > Code Generation
Tool Settings - RS08 Assembler > Code Generation

The following table lists and describes the Code Generation options for RS08 Assembler.

Table 1. Tool Settings - RS08 Assembler > Code Generation Options
Option Description
Associate debug information to assembly source file ( -Asmdbg) Passes the assembly source file name information to DWARF sections. When the output .abs file is debugged, the actual assembly source file is displayed instead of intermediary <filename>.dbg file.