HCS08 Assembler > Language > Compatibility modes

The following image shows the Compatibility modes panel.

Figure 1. Tool Settings - HCS08 Assembler > Language > Compatibility modes
Tool Settings - HCS08 Assembler > Language > Compatibility modes

The following table lists and describes the compatibility mode options for HCS08 Assembler.

Table 1. Tool Settings - HCS08 Assembler > Language > Compatibility mode Options
Option Description
Select all ( -Compat) Check to enable all compatibility mode options.
Symbol prefixes ( -Compat=s) With this suboption, the Assembler accepts "pgz:" and "byte:" prefixed for symbols in XDEFs and XREFs. They correspond to XREF.B or XDEF.B with the same symbols without the prefix.
Ignore FF character at line start Symbol prefixes ( -Compat=f) With this suboption, an otherwise improper character recognized from feed character is ignored.
Alternate comment rules ( -Compat=c) With this suboption, comments implicitly start when a space is present after the argument list. A special character is not necessary. Be careful with spaces when this option is given because part of the intended arguments may be taken as a comment. However, to avoid accidental comments, the Assembler does issue a warning if such a comment does not start with a "*" or a ";".
Support FOR directive ( -Compat=b) With this suboption, the Assembler supports a FOR - Repeat assembly block assembly directive to generate repeated patterns more easily without having to use recursive macros.
Add some additional directives ( -Compat=a) With this suboption, some additional directives are added for enhanced compatibility. The Assembler actually supports a SECT directive as an alias of the usual SECTION - Declare Relocatable Section assembly directive. The SECT directive takes the section name as its first argument.
Operator != means equal ( -Compat==) The Assembler takes the default value of the != operator as not equal, as it is in the C language. For compatibility, this behavior can be changed to equal with this option. Because of the risks involved with this option for existing code, a message is issued for every != which is treated as equal.
Support $ character in symbols ( -Compat=$) With this suboption, the Assembler supports to start identifiers with a $ sign.
Support additional ! symbols ( -Compat=!) The following additional operators are defined when this option is used:
  • !^: exponentiation
  • !m: modulo
  • !@: signed greater or equal
  • !g: signed greater
  • !%: signed less or equal
  • !t: signed less than
  • !$: unsigned greater or equal
  • !S: unsigned greater
  • !&: unsigned less or equal
  • !l: unsigned less
  • !n: one complement
  • !w: low operator
  • !h: high operator
Note: The default values for the following ! operators are defined:
  • !.: binary AND
  • !x: exclusive OR
  • !+: binary OR