Assembler Build Properties Panels

The following sections describe how to configure the HCS08 Assembler Build Properties Panels and RS08 Assembler Build Properties Panels. These panels are part of the project's build properties settings, which are managed in the Properties dialog box. To access these panels, proceed as follows:

  1. Select the project for which you want to set the build properties, in the CodeWarrior Projects view.
  2. Select Project > Properties.

    The Properties for <project> dialog box appears.

  3. Expand the C/C++ Build tree node and select Settings.

The various settings for the build tools appears in the right panel.

If not, click the Tool Settings tab. If you have selected an HCS08 project, the HCS08 tool settings page appears.

If you have selected an RS08 project, the RS08 tool settings page appears.

The options are grouped by tool, such as General options, Linker options, Assembler options, and Assembler options. Depending on the build properties you wish to configure, select the appropriate option in the Tool Settings tab page.