[DISABLED, INFORMATION, WARNING, ERROR]
The absolute expression specified as initialization value for a block defined using DCB is too big. This message is generated when the initial value specified in a DCB.B directive cannot be coded on a byte. In this case the value used to initialize the constant block will be truncated to a byte value.
constSec: SECTION
; ...
label1: DCB.B 2, 312
; ...
In the previous example, the constant block is initialized with the value $38 (= 312 & $FF)
To avoid this warning, modify the initialization value to a byte value.
constSec: SECTION
; ...
label1: DCB.B 2, 56
; ...