Including RTOS Functions in CDE RTOS GUI

The RTOS component produces RTOS-specific function calls into LDD-generated code to perform the operations, such as memory allocation and deallocation, enter/exit critical sections, and OS-specific include declaration. However, there is one special case, where a function must be declared: ISRs. The CDE's RTOS GUI requires four different values for every function:

The only difference between entering parameters for an ISR declaration and rest of the RTOS function in RTOS GUI is that when declaring an ISR, the Add Parameter button adds entries in pairs. This confirms that this is a function declaration where the input parameters are declared in the form of <variable_type1> <variable_name1>, <variable_type2> <variable_name2>...

For more information, refer to the Creating RTOS Component topic.