Interrupt Vector Table Handling

RTOS adapter provides an abstraction of settings of interrupt vectors. If RTOS provides dynamic reconfiguration of vector table, maps to this RTOS functionality. If vector table is static, Processor Expert can generate it according to the requests. There are also subroutines for generation of ISR function definition and declaration.