At some point you may be required to reprogram the USB TAP probe's firmware image stored in its flash EPROM. Typically this occurs when you are installing an update to existing software, and the release letter specifies a later version of probe core software.
CodeWarrior_Installation\ccs\bin\ccs.exe
This will launch CCS and add a CCS icon (see below figure) to your taskbar. Double-click that icon in the taskbar to open the command window.
CodeWarrior_Installation/ccs/bin/ccs
This will launch CCS and open the command window automatically.
delete all updateutap [serial_number]
The serial_number parameter is the serial number of your USB TAP probe, which is shown on the bottom of the device. If you have only one USB TAP probe connected to your host machine, you do not need to specify the serial_number parameter. Output similar to the following will be displayed.
USB TAP Loader current software ver. {1.0}
Sending code to USB TAP - please wait
*** WARNING ***
DO NOT UNPLUG YOUR USB TAP: Doing so will render your USB
TAP non-functional and require factory reprogramming.
Please wait until the flashing Yellow/Green TGT STATUS light
turns off.
*** WARNING ***