JTAG/COP connector information

The CodeWarrior USB TAP JTAG/COP probe has a 16-pin connector which automatically supports target signal levels from 1.8V to 3.3V.

The following figure shows the pin assignments of the probe JTAG/COP connector.

The following table lists JTAG/COP signal names, direction, pin numbers, descriptions, and drive capabilities for the probe JTAG/COP connector.

Note: All JTAG/COP signals must meet accepted standards for JTAG/COP signal design. To ensure proper and stable operation between the USB TAP probe and the target, the JTAG/COP signals must meet the requirements listed in Table A.2.
Figure 1. USB TAP probe for JTAG/COP connector pin assignments

USB TAP Probe for JTAG/COP Connector Pin Assignments

Table 1. USB TAP probe for JTAG/COP signal directions
JTAG/COP pin Signal mnemonic Signal direction Description
1 TDO From target system 30pF load
2 QACK From USB TAP probe connector 100Ohm pull-down
3 TDI From USB TAP probe connector 50mA driver
4 TRST From USB TAP probe connector 50mA driver
5 HALTED Bi-directional Open-drain, 100Ohm to ground when asserted by USB TAP probe, 35pF load when not asserted
6 TGT PWR From target 2MOhm pull-down, plus 0.01uF load
7 TCK From USB TAP probe connector 50mA driver
8 CKSI From USB TAP probe connector 50mA driver
9 TMS From USB TAP probe connector 50mA driver
10 No Connect - n/a -  
11 SRST Bi-directional Open-drain. 100Ohm to ground when asserted by USB TAP, 35pF load when not asserted1
12 No Connect - n/a -  
13 HRST Bi-directional Open-drain. 100Ohm to ground when asserted by USB TAP, 35pF load when not asserted1
14 No Connect - n/a -  
15 CKSO From target 30pF load1
16 GND - n/a -  

The following table provides a general description of each JTAG/COP signal and the operational requirements.

Table 2. USB TAP probe for JTAG/COP signal recommendations/requirements
JTAG/COPpin Signal mnemonic Requirement
1 TDO Must be wired to the target processor. TDO is an output from the target processor and an input to the USB TAP probe. The TDO trace run should be kept short and maintain a "two-signal-width" spacing from any other parallel dynamic signal trace. TDO should have a series termination resistor located near the target processor.
2 QACK May be wired to the target processor. QACK is an input to most Power Architecture processors and must remain low while the USB TAP probe is connected to the target. The USB TAP probe connects this signal internally to the JTAG/COP GND pin (16) through a 100Ohm resistor.
3 TDI Must be wired to the target processor. The USB TAP probe drives the TDI output with up to 50mA. The TDI trace should be kept short and maintain a "two-signal-width" spacing from any other parallel dynamic signal trace. TDI should have an RC termination option at the processor.
4 TRST Must be wired to the target processor. The USB TAP probe drives the TRST output with up to 50mA. To gain control of the processor, the USB TAP probe negates TRST approximately 250 milliseconds before negation of HRST. This allows the USB TAP probe to issue COP commands through the JTAG/COP interface and gain control of the processor upon negation of HRST. The TRST trace run should be kept short and maintain a "two-signal-width" spacing from any other parallel dynamic signal trace.
5 HALTED Need not be wired to the target. The USB TAP probe does not currently use this signal.
6 TGT PWR Must be wired to the target. The USB TAP probe uses this signal to determine if power is applied to the target. This signal is also used as a voltage reference for the signals driven by the USB TAP probe (CKSI, TRST, TCK, TMS, TDI). TGT PWR (pin 6) should be connected to target Vcc through a 1KOhm pull-up.
7 TCK Must be wired to the target processor. The USB TAP probe drives the TCK output with up to 50mA. The TCK trace run should be kept as short as possible and maintain a "two-signal-width" spacing from any other parallel dynamic signal trace.
8 CKSI Need not be wired to the target.The USB TAP does not currently use this signal.
9 TMS Must be wired to the target processor. The USB TAP drives the TMS output with up to 50mA. TMS should be kept as short as possible and maintain a "two-signal-width" spacing from any other parallel dynamic signal trace. TMS should have a termination option at the processor.
10 No Connect Not required for emulation.
11 SRST May be wired to the target processor. During reset, the USB TAP drives SRST to ground through a 100Ohm resistor.
12 No Connect Not required for emulation.
13 HRST Must be wired to the target processor. During reset, the USB TAP probe drives HRST to ground through a 100Ohm resistor.
14 No Connect Not required for emulation.
15 CKSO Should be wired to the target processor. The USB TAP senses CKSO to determine if the processor halted execution in a checkstop state.
16 GND Must be wired to the target. GND is connected directly to the ground inside the USB TAP probe.

Notes specific to MPC8240, MPC8241, and MPC8245

CKSO is not available on the MPC8240, MPC8241, or MPC8245 processors.

SRST can be deselected in favor of the SDMA12 signal used for Extended Addressing (except on the MPC8240 processor).

QACK is an output signal only, so it need not be connected to the COP header.

The USB TAP probe fully supports the MPC8240, MPC8241, and MPC8245 processors despite the absence of the signals mentioned above.

Signal width example

Signal line 'A' is 0.005 mil. An adjacent dynamic signal line 'B' should maintain a "two-signal-width" distance from signal line 'A'. So that from the center of line 'A' to the center of line 'B', there should be 0.0025 + 0.005 + 0.005 + 0.0025 = 0.015mil.

Target bias should maintain "one-signal-width" spacing from the signal.

1 4.7KOhm pull-up to buffered TGT PWR.