When the USB TAP probe is powered on, it performs a brief self-test that displays a test pattern on both the Run/Pause and Transmit/Receive LEDs. After the self-test completes, the status LED (labeled RUN/PAUSE) indicates the state of execution on the target device as follows:
For the definition of run and pause modes, see Run/Pause/Mixed Mode States.