The following figures show the various LEDs and connectors of the USB TAP probe.
When the USB TAP probe is powered on, it performs a brief self-test that displays a test pattern on both the Run/Pause and Transmit/Receive LEDs. After the self-test completes, the status LED (labeled RUN/PAUSE) indicates the state of execution on the target device as follows:
For the definition of run and pause modes, see Run/Pause/Mixed mode states topic.
When the USB TAP probe is powered on, it performs a brief self-test that displays a test pattern on both the Run/Pause and Transmit/Receive LEDs. After the self-test completes, the transmit/receive LED (labeled TX/RX) indicates the state of the USB interface as follows:
The USB interface consists of a USB type B connector that connects directly to the USB cable provided.
The debug port connector consists of a 5.5 inch ribbon cable with the appropriate debug connector attached. The ribbon cable has a red stripe down one side to indicate the location of pin 1.