USB TAP probe system startup

This section explains how to start using the USB TAP probe and the debugger.

Before starting the USB TAP probe, make sure you have:

Starting USB TAP probe

  1. Apply power to the target system.
  2. Start the debugger.

    LEDs are provided to indicate the status of the USB TAP probe. For description of the various indicators, see Hardware specifications topic.

You are now ready to begin your debug session. For information on using the CodeWarrior debugger, see Targeting manual..