For CodeWarrior tools that do not support creating multiple USB TAP probe connections in the IDE, create a CCS Remote Connection for each, using unique port numbers. Then for each device, start the CCS Console and configure the connection, specifying the probe serial number. Tools that support creation of only one USB TAP probe connection within the IDE will not provide an option for entering the device serial number.
Tip:
If the CodeWarrior IDE variant requires using separate CCS sessions to connect to each USB TAP probe, and you would like the setup steps to run automatically when you launch the debugger, edit the
\ccs\bin\ccs.cfg file with the new commands.
Tip:
If you are using a USB hub to connect the USB TAP probe to the host computer, be sure to use a powered hub.
Tip:
To set up the debug connection, you will need to know the 8-digit USB TAP probe serial number, located on a label on the bottom of the device.