Specifies the addressing mode and location of object code for functions.
#pragma CODE_SEG [ modifier ] [ name ]
#pragma CODE_SEG DEFAULT
modifier
This optional parameter specifies the addressing mode to use:
name
A section name. You must use a section name defined in your project's linker command file.
To specify the section in which to store a function and the addressing mode to refer to it, place this pragma before the function definition. Use this pragma when porting source code from HC08 architectures to ColdFire V1 architectures.
Use DEFAULT to use the parameters specified by the previous use of this pragma.
The following listing shows an example.
void f(void); void h(void); /* Use far addressing to refer to this function. */ /* Store function in section "text". */ #pragma CODE_SEG __FAR_SEG text void f(void){ h(); } /* Use near addressing to refer to this function. */ /* Store function in section "MYCODE2". */ #pragma CODE_SEG __NEAR_SEG MYCODE2 void h(void){ f(); } /* Use previous pragma CODE_SEG parameters: */ /* __FAR_SEG text */ #pragma CODE_SEG DEFAULT