If the Simulator or Debugger cannot be launched, check the settings in the project's launch configuration. For more information on launch configurations and their settings, refer to the Mircocontrollers Version 10.x Targeting Manual. Note: You can view and modify the project's launch configurations from the IDE's Run Configurations or Debug Configurations dialog box. To open these dialog boxes, select Run > Run Configurations or Run > Debug Configurations.