Stores data to reduce data size instead of improving execution performance.
#pragma pack()
#pragma pack(0 | n | push | pop)
n
One of these integer values: 1, 2, 4, 8, or 16.
Use this pragma to align data to use less storage even if the alignment might affect program performance or does not conform to the target platform's application binary interface (ABI).
If this pragma's argument is a power of 2 from 1 to 16, the compiler will store subsequent data structures to this byte alignment.
The push argument saves this pragma's setting on a stack at compile time. The pop argument restores the previously saved setting and removes it from the stack. Using this pragma with no argument or with 0 as an argument specifies that the compiler will use ABI-conformant alignment.
Not all processors support misaligned accesses, which could cause a crash or incorrect results. Even on processors which allow misaligned access, your program's performance might be reduced. Your program may have better performance if it treats the packed structure as a byte stream, then packs and unpacks each byte from the stream.