Uses a safer variation of strength reduction optimization.
#pragma opt_strength_reduction_strict on | off | reset
Like the opt_strength_reduction pragma, this setting replaces multiplication instructions that are inside loops with addition instructions to speed up the loops. However, unlike the regular strength reduction optimization, this variation ensures that the optimization is only applied when the array element arithmetic is not of an unsigned type that is smaller than a pointer type.
This pragma does not correspond to any panel setting. The default varies according to the compiler.