ipa_inline_max_auto_size

Determines the maximum complexity for an auto-inlined function.

Syntax
  #pragma ipa_inline_max_auto_size (intval)  
Parameters

intval

The intval value is an approximation of the number of statements in a function, the current default value is 500, which is approximately equal to 100 satement function. Selecting a zero value will disable the IPA auto inlining.

Remarks

The size of the code objects that are not referenced by address and are only called once is specified above a certain threshold using this pragma, preventing them from being marked as inline.