Controls how included files are treated when #pragmaonce is enabled.
#pragma syspath_once on | off | reset
When this pragma and pragma once are set to on, the compiler distinguishes between identically-named header files referred to in #include <file-name> and #include "file-name".
When this pragma is off and pragma once is on, the compiler will ignore a file that uses a
#include <file-name>
directive if it has previously encountered another directive of the form
#include "file-name"
for an identically-named header file.
shows an example.
This pragma does not correspond to any panel setting. By default, this setting is on.
#pragma syspath_once off #pragma once on /* Include all subsequent files only once. */ #include "sock.h" #include <sock.h> /* Skipped because syspath_once is off. */