Controls the generation of debugger symbol information for subsequent functions.
#pragma sym on | off | reset
The compiler pays attention to this pragma only if you enable the debug marker for a file in the IDE project window. If you disable this pragma, the compiler does not put debugging information into the source file debugger symbol file (SYM or DWARF) for the functions that follow.
The compiler always generates a debugger symbol file for a source file that has a debug diamond next to it in the IDE project window. This pragma changes only which functions have information in that symbol file.
This pragma does not correspond to any panel setting. By default, this pragma is enabled.