cpp_extensions

Controls language extensions to ISO/IEC 14882-2003 C++.

Syntax
  #pragma cpp_extensions on | off | reset  
Remarks

If you enable this pragma, you can use the following extensions to the ISO/IEC 14882-2003 C++ standard that would otherwise be invalid: