require_prototypes

Controls whether or not the compiler should expect function prototypes.

Syntax
  #pragma require_prototypes on | off | reset  
Remarks

This pragma affects only non-static functions.

If you enable this pragma, the compiler generates an error message when you use a function that does not have a preceding prototype. Use this pragma to prevent error messages, caused by referring to a function before you define it. For example, without a function prototype, you might pass data of the wrong type. As a result, your code might not work as you expect even though it compiles without error.

In the following listing, the main() function calls PrintNum() with an integer argument, even though the PrintNum() takes an argument of the type float.

Listing: Unnoticed Type-mismatch
#include <stdio.h>
void main(void)

{

  PrintNum(1);  /* PrintNum() tries to interpret the 

                   integer as a float. Prints 0.000000. */

}

void PrintNum(float x)

{

    printf("%f\n", x);

}

When you run this program, you could get this result:

  0.000000  

Although the compiler does not complain about the type mismatch, the function does not give the result you desired. Since PrintNum() does not have a prototype, the compiler does not know how to generate the instructions to convert the integer, to a floating-point number before calling PrintNum(). Consequently, the function interprets the bits it received as a floating-point number and prints nonsense.

A prototype for PrintNum(), as in the following listing, gives the compiler sufficient information about the function to generate instructions to properly convert its argument to a floating-point number. The function prints what you expected.

Listing: Using a Prototype to Avoid Type-mismatch
#include <stdio.h>
void PrintNum(float x); /* Function prototype. */

void main(void)

{

    PrintNum(1);        /*  Compiler converts int to float.

}                           Prints 1.000000. */

void PrintNum(float x)

{

    printf("%f\n", x);

}

In other situations where automatic conversion is not possible, the compiler generates an error message if an argument does not match the data type required by a function prototype. Such a mismatched data type error is easier to locate at compile time than at runtime.