Optimization level exported as a predefined macro.
__optlevel0
__optlevel1
__optlevel2
__optlevel3
__optlevel4
Using these macros, user can conditionally compile code for a particular optimization level. The following table lists the level of optimization provided by the __optlevelx macro.
| Macro | Optimization Level |
|---|---|
| __optlevel0 | O0 |
| __optlevel1 | O1 |
| __optlevel2 | O2 |
| __optlevel3 | O3 |
| __optlevel4 | O4 |
The listing below shows an example of __optlevelx macro usage.
int main() { #if __optlevel0 ... // This code compiles only if this code compiled with Optimization level 0 #elif __optlevel1 ... // This code compiles only if this code compiled with Optimization level 1 #elif __optlevel2 ... // This code compiles only if this code compiled with Optimization level 2 #elif __optlevel3 ... // This code compiles only if this code compiled with Optimization level 3 #elif __optlevel4 ... // This code compiles only if this code compiled with Optimization level 4 #endif }