Updating Precompiled File Automatically

Use the CodeWarrior IDE's project manager to update a precompiled header automatically. The IDE creates a precompiled file from a source code file during a compile, update, or make operation if the source code file meets these criteria:

The IDE uses the build target's settings to preprocess and precompile files.