Variable length arrays are supported within local or function prototype scope, as required by the ISO/IEC 9899-1999 ("C99") standard. The following listing shows an example.
#pragma c99 on void f(int n) { int arr[n]; /* ... */ }
While the example shown in the following figure generates an error message.
#pragma c99 on int n; int arr[n]; // ERROR: variable length array // types can only be used in local or // function prototype scope.
A variable length array cannot be used in a function template's prototype scope or in a local template typedef, as shown in the following listing.
#pragma c99 on template<typename T> int f(int n, int A[n][n]); { }; // ERROR: variable length arrays // cannot be used in function template prototypes // or local template variables