The CodeWarrior compiler accepts many of the extensions to the C language that the GCC (GNU Compiler Collection) tools allow. Source code that uses these extensions does not conform to the ISO/IEC 9899-1990 C ("C90") standard.