-sreceol

Specifies the end-of-line style to use in an S-record file.

Syntax
  -sreceol keyword

  

The options for the keyword are:

mac

Uses the Mac OS®-style end-of-line format.

dos

Uses the Microsoft® Windows®-style end-of-line format. This is the default choice.

unix

Uses a UNIX-style end-of-line format.

Remarks

This option also generates an S-record file if the -srec option has not already been specified.

This is a linker option.