-show

Specifies the information to list in a disassembly.

Syntax
  -show keyword[,...]

  

The options for the keyword are:

only | none

Shows no disassembly. Begins a list of options with only or none to prevent the default information from appearing in the disassembly.

all

Shows everything. This is default.

[no]code | [no]text

Shows disassembly of the code sections. This is default.

[no]comments

Shows comment field in the code. Implies -show code. This is default.

[no]extended

Shows the extended mnemonics. Implies -show code. This is default.

[no]data

Shows data with -show verbose, shows hex dumps of the sections. This is default.

[no]debug | [no]sym

Shows the symbolics information. This is default.

[no]exceptions

Shows the exception tables. Implies -show data. This is default.

[no]headers

Shows the ELF headers. This is default.

[no]hex

Shows addresses and opcodes in the code disassembly. Implies -show code. This is default.

[no]names

Shows the symbol table. This is default.

[no]relocs

Shows resolved relocations in the code and relocation tables. This is default.

[no]source

Shows source in the disassembly. Implies -show code, with -show verbose, displays the entire source file in the output, else shows only four lines around each function. This is default.

[no]xtables

Shows the exception tables. This is default.

[no]verbose

Shows verbose information, including the hex dump of program segments in the applications. This is default.

Remarks

This is a linker option.