Specifies a library selection.
-lavender keyword[,...]
The options for keyword are:
model=string
Selects a library model for string, maximum length is 511 chars. The default is none.
print=string
Selects a printf formatter for string, maximum length is 511 chars;. The default is none.
scan=string
Selects a scanf formatter for string, maximum length is 511 chars. The default is none.
io=string
Selects an IO mode for string, maximum length is 511 chars. The default is none.
This is a library option.