WRITES0COMMENT

Inserts an S0 comment record into an S-record file.

  WRITES0COMMENT "comment"

  
Parameter

comment

Comment text: a string of alphanumerical characters 0-9, A-Z, and a-z, plus space, underscore, and dash characters. Double quotes must enclose the comment string. (If you omit the closing double-quote character, the linker tries to put the entire LCF into the S0 comment.)

Remarks

This command, valid only in an LCF sections segment, creates an S0 record of the form:

  S0aa0000bbbbbbbbbbbbbbbbdd
  
  

This command does not null-terminate the ASCII string.

Within a comment string, do not use these character sequences, which are reserved for LCF comments: # /* */ //

Example

This example shows that multi-line S0 comments are valid:

  WRITES0COMMENT "Line 1 comment

  
  Line 2 comment"