Creates the exception table index in the output file.
EXCEPTION
Only C++ code requires exception tables. To create an exception table, add the EXCEPTION command, with symbols __exception_table_start__ and __exception_table_end__, to the end of your code section segment, just as Listing: Creating an Exception Table shows. (At runtime, the system identifies the values of the two symbols.)
The following listing shows the code for creating an exception table.
__exception_table_start__ = .; EXCEPTION __exception_table_end__ = .;