Controls the use of non-standard ISO/IEC 9899-1990 ("C90") language features.
-strict on | off
If this option is on, the compiler generates an error message when it encounters some CodeWarrior extensions to the C language defined by the ISO/IEC 9899-1990 ("C90") standard:
The default setting is off.