ColdFire Compiler Build Settings Panels

The following sections describe the settings panels that configure the build tool options. These panels are part of the project's build properties settings, which are managed in the Properties for <project> dialog box. To access these panels, proceed as follows:

  1. Select the project for which you want to set the build properties, in the CodeWarrior Projects view.
  2. Select Project > Properties from the IDE menu bar.

    A Properties for <project> dialog box appears.

  3. Expand the C/C++ Build tree control, and then select the Settings option.

    The settings for the build tools are displayed in the right panel of the Properties for <project> dialog box. If not, click on the Tool Settings tab.

    Figure 1. Project's Properties Dialog Box
    Project's Properties Dialog Box

The options are grouped by tool, such as general options, linker options, ColdFire compiler options, and so on. Scroll down the list, and click on the option whose settings you wish to examine and modify.

The following table lists the build properties specific to developing software for ColdFire.

The properties that you specify in these panels, apply to the selected build tool on the Tool settings page of the Properties for <project> dialog box.