ColdFire Compiler

Use this panel to specify the command, options, and expert settings for the build tool compiler. Additionally, the ColdFire Compiler tree control includes the general, include file search path settings. The following figure shows the ColdFire Compiler settings.

Figure 1. Tool Settings - ColdFire Compiler
Tool Settings - ColdFire Compiler

The following table lists and describes the compiler options for the ColdFire connection.

Table 1. Tool settings - ColdFire Compiler Options
Option Description
Command Shows the location of the compiler executable file. Specify additional command line options for the compiler; type in custom flags that are not otherwise available in the UI.
All options Shows the actual command line the compiler will be called with.

Expert settings

Command line pattern

Shows the expert settings command line parameters; default is ${COMMAND} ${FLAGS}${OUTPUT_FLAG}${OUTPUT_PREFIX}${OUTPUT} ${INPUTS}.