Creating Project

This chapter covers the primary method to create a project with the CodeWarrior Development Studio for Microcontrollers, Version 10.x.

For information on creating and compiling a project using the CodeWarrior IDE, refer to the Creating and Managing Project Using CodeWarrior IDE section of this chapter.

Note: Information on the other build tools can be found in User Guides included with the CodeWarrior Suite and are located in the Help folder for the CodeWarrior installation. The default location of this folder is: C:\Freescale\CW MCU v10.x\MCU\Help