When the GCC extensions setting is on, the sizeof() operator computes the size of function and void types. In both cases, the sizeof() operator evaluates to 1. The ISO/IEC 9899-1990 C Standard ("C90") does not specify the size of the void type and functions. The following listing shows an example.
int f(int a) { return a * 10; } void g(void) { size_t voidsize = sizeof(void); /* voidsize contains 1 */ size_t funcsize = sizeof(f); /* funcsize contains 1 */ }