C5912: Code in 'if' and 'else' part are the same

[DISABLE, INFORMATION , WARNING, ERROR]

Description

The Compiler has detected that the code in the 'if' and the code in the 'else' part of an 'if-else' construct is the same. Because regardless of the condition in the 'if' part, the executed code is the same, so the compiler replaces the condition with 'TRUE' if the condition does not have any side effects. There is always a couple of this message, one for the 'if' part and one for the 'else' part. This message may be generated during tree optimizations (Option -Ont to switch it off).

Example
  if (condition) {  // replaced with 'if (1) {'

  
    statements;  // message C5912 here ...

  
  } else {

  
    statements;  // ... and here

  
  }

  
Tips

Check your code why both parts are the same. Maybe different macros are used in both parts which evaluates to the same values.