C5300: Limitation: code size '<actualSize>' > '<limitSize>' bytes

[ERROR]

Description

You have a limited version of the compiler or reached the limitation specified in the license file. The actual demo limitation is 1024 bytes of code for 8/16bit targets and 3KByte for 32bit targets (without a license file). Depending on the license configuration, the code size limit may be specified in the license file too.

Tips

Check if you have enough licenses if you are using a floating license configuration. Check for the correct location of the license file. Get a license for a full version of the compiler, or for a code size upgrade.