[WARNING]
A pragma was not used by the compiler. This may have different reasons: the pragma is intended for a different compiler by a typing mistake, the compiler did not recognize a pragma. Note that pragma names are case sensitive. there was no context, a specific pragma could take some action The segment pragma DATA_SEG, CODE_SEG, CONST_SEG and their aliases never issue this warning, even if they are not used.
#pragma TRAP_PROG
// typing mistake: the interrupt pragma is called TRAP_PROC
void Inter(void) {
...
}
Investigate this warning carefully. This warning can be mapped to an error if only pragmas are used which are known.