C3202: Ident too long

[FATAL]

Description

An identifier was longer than allowed. The compiler supports identifiers with up to 16000 characters. Note that the limits of the linker/debugger may be smaller. The 16000 characters are in respect of the length of the identifier in the source. A name mangled C++ identifier is only limited by available memory.

Tips

Do not use such extremely large names!