C1857: Access out of range

[DISABLE, ERROR, WARNING , INFORMATION]

Description

The compiler has detected that there is an array access outside of the array bounds. This is legal in ANSI-C/C++, but normally it is a programming error. Check carefully such accesses that are out of range. This warning does not check the access, but also taking the address out of an array. However, it is legal in C to take the address of one element outside the array range, so there is no warning for this. Because array accesses are treated internally like address-access operations, there is no message for accessing on element outside of the array bounds.

Example
  char buf[3], *p;

  
  p = &buf[3]; // no message!

  
  buf[4] = 0;  // message