[ERROR]
A break was made outside of an iteration-statement.
int i;
void f(void) {
int res;
for (i=0; i < 10; i++ )
res=f(-1);
if (res == -1)
break;
printf("%d\n", res);
}
The break must be done inside an iteration-statement. Check for the correct number of open braces.