C1133: Such an initialization requires STATIC CONST INTEGRAL member

[ERROR]

Description

A static CONST member of integral type may be initialized by a constant expression in its member declaration within the class declaration.

Example
  int e = 0;

  
  class A{

  
  public:

  
    static int a = 1; // ERROR: non-const initialized

  
    const int b = 2; // ERROR: non-static initialized

  
    static const float c = 3.0;// ERROR: non-integral

  
                               // initializer

  
  static const int d = e; // ERROR: non-const initializer

  
    // ...

  
  };

  
Tips
  class A{

  
  public:

  
    static const int a = 5; // Initialization

  
    // ...

  
  };

  
  const int A::a;             // Definition

  

or the other way round:

  class A{

  
  public:

  
    static const int a;     // Definition

  
    // ...

  
  };

  
  const int A::a = 5;         // Initialization