Messages of HC08 Back End

Messages of HC08 Back End The following sections contains message descriptions specific for the HC08 compiler. All messages specific for the HC08 have a number of the form C18XXX, where XXX is a different number for every message. Up to the compiler version 5.0.7, there is also a set of messages with numbers C20XXX (ICG based technology).