A ROM Library requires a very simple startup file, containing only the definition from the startup structure. Usually a ROM library startup file looks as follows:
#include "startup.h"
/* read-only: _startupData is allocated in ROM and ROM Library PRM File */
struct _tagStartup _startupData;
You must generate a PRM file to set code placement in RAM. Because the compiler generates absolute code, the linker must know the final location of the code to generate correct code for the function call.
In the PRM file, you must:
The following listing shows a PRM file that copies and executes code at address 0x7000.
LINK fiboram.abs AS ROM_LIB NAMES myFibo.o start.o END SECTIONS MY_RAM = READ_WRITE 0x4000 TO 0x43FF; MY_ROM = READ_ONLY 0x7000 TO 0xBFFF; /* Dest. Address in RAM area */ PLACEMENT DEFAULT_ROM, ROM_VAR, STRINGS INTO MY_ROM; DEFAULT_RAM INTO MY_RAM; END ENTRIES myMain END