realloc()

This function is Hardware-specific implementation. It is not implemented in this Compiler.

Syntax
  #include <stdlib.h>

  
  void *realloc(void *ptr, size_t size);

  
Description

realloc() changes the size of a memory block, preserving its contents. ptr must be a pointer returned by calloc(), malloc(), realloc(), or NULL. In the latter case, realloc() is equivalent to malloc().

If the new memory block size is smaller than the old size, realloc() discards the memory at the end of the block. If size is zero (and ptr is not NULL), realloc() frees the whole memory block.

If there is not enough memory to perform the realloc(), the old memory block is left unchanged, and realloc() returns NULL. Do not use realloc() in interrupt routines as the default implementation is not reentrant.

Return

realloc() returns a pointer to the new memory block. If the operation cannot be performed, realloc() returns NULL.

See also

free()