This is a file I/O function, also hardware dependent. It is not implemented in this Compiler.
#include <stdio.h>
long ftell(FILE *f);
ftell() returns the current file position. For binary files, this is the byte offset from the beginning of the file; for text files, do not use this value except as an argument to fseek().
-1, if an error occurred; otherwise the current file position.