The High-Level Inline (HLI) Assembler makes full use of the target processor properties from within a C program. There is no need to write a separate assembly file, assemble it, and later bind it with the rest of the application written in ANSI-C with the inline assembler. The Compiler does all the work. For detailed information, refer to the Freescale HC(S)08 Family Reference Manual.
This chapter lists the following topics: