This section describes the internal Compiler limitations. Some stack limitations depend on the operating system used. For example, in some operating systems, limits depend on whether the compiler is a 32-bit compiler running on a 32-bit platform (for example, Windows XP), or a 16-bit Compiler running on a 16-bit platform (for example, Windows for Workgroups).
The ANSI-C column in the following below shows the recommended limitations of ANSI-C (5.2.4.1 in ISO/IEC 9899:1990 (E)) standard. These limitations are only guidelines and do not determine compliance. The Implementation column shows the actual implementation value and the possible message number. A dash in the Implementation column means that there is no information available for this topic.
| Limitation | Implementation | ANSI-C |
|---|---|---|
| Nesting levels of compound statements, iteration control structures, and selection control structures | 256 (C1808) | 15 |
| Nesting levels of conditional inclusion | - | 8 |
| Pointer, array, and function decorators (in any combination) modifying an arithmetic, structure, union, or incomplete type in a declaration | - | 12 |
| Nesting levels of parenthesized expressions within a full expression | 32 (C4006) | 32 |
| Number of initial characters in an internal identifier or macro name | 32,767 | 31 |
| Number of initial characters in an external identifier | 32,767 | 6 |
| External identifiers in one translation unit | - | 511 |
| Identifiers with block scope declared in one block | - | 127 |
| Macro identifiers simultaneously defined in one translation unit | 655,360,000 (C4403) | 1024 |
| Parameters in one function definition | - | 31 |
| Arguments in one function call | - | 31 |
| Parameters in one macro definition | 1024 (C4428) | 31 |
| Arguments in one macro invocation | 2048 (C4411) | 31 |
| Characters in one logical source line | 2^31 | 509 |
| Characters in a character string literal or wide string literal (after concatenation) | 8196 (C3301, C4408, C4421) | 509 |
| Size of an object | 32,767 | 32,767 |
| Nesting levels for #include files | 512 (C3000) | 8 |
| Case labels for a switch statement (excluding those for any nested switch statements) | 1000 | 257 |
| Data members in a single class, structure, or union | - | 127 |
| Enumeration constants in a single enumeration | - | 127 |
| Levels of nested class, structure, or union definitions in a single struct declaration list | 32 | 15 |
| Functions registered by atexit() | - | n/a |
| Direct and indirect base classes | - | n/a |
| Direct base classes for a single class | - | n/a |
| Members declared in a single class | - | n/a |
| Final overriding virtual functions in a class, accessible or not | - | n/a |
| Direct and indirect virtual bases of a class | - | n/a |
| Static members of a class | - | n/a |
| Friend declarations in a class | - | n/a |
| Access control declarations in a class | - | n/a |
| Member initializers in a constructor definition | - | n/a |
| Scope qualifications of one identifier | - | n/a |
| Nested external specifications | - | n/a |
| Template arguments in a template declaration | - | n/a |
| Recursively nested template instantiations | - | n/a |
| Handlers per try block | - | n/a |
| Throw specifications on a single function declaration | - | n/a |
The table below shows other limitations which are not mentioned in an ANSI standard:
| Limitation | Description |
|---|---|
| Type Declarations | Derived types must not contain more than 100 components. |
| Labels | There may be at most 16 other labels within one procedure. |
| Macro Expansion | Recursive macros expansion is limited to 70 (16-bit OS) or 2048 (32-bit OS) recursive expansions (C4412). |
| Include Files | The total number of include files is limited to 8196 for a single compilation unit. |
| Numbers | Maximum of 655,360,000 different numbers for a single compilation unit (C2700, C3302). |
| Goto | M68000 products only: Maximum of 512 Gotos for a single function (C15300). |
| Parsing Recursion | Maximum of 1024 parsing recursions (C2803). |
| Lexical Tokens | Limited by memory only (C3200). |
| Internal IDs | Maximum of 16,777,216 internal IDs for a single compilation unit (C3304). Internal IDs are used for additional local or global variables created by the Compiler (for example, by using CSE). |
| Code Size | Code size is limited to 32KB for each single function. |
| Filenames | Maximum length for filenames (including path) is 128 characters for 16-bit applications or 256 characters for Win32 applications. UNIX versions support filenames without the path of 64 characters in length and 256 characters with the path. Paths may be 96 characters on 16-bit PC versions, 192 characters on UNIX versions or 256 characters on 32-bit PC versions. |