The Compiler supports two IEEE floating-point formats: IEEE32 and IEEE64. The processor may also support a DSP format. The following listing shows these three formats.
Floats are implemented as IEEE32 and doubles as IEEE64. This may vary for a specific Backend, or possibly neither format is supported. Refer to HC(S)08 Backend for details, default settings, and supported formats.
The topics covered here are as follows: