An enum in C has a unique name and a defined value (refer the following listing).
#pragma CREATE_ASM_LISTING ON enum { E1=4, E2=47, E3=-1*7 };
The Compiler generates enums as EQU directives (refer the following listing).
E1 EQU $4 E2 EQU $2F E3 EQU $FFFFFFF9